AOUT#.VALUE

Description

AOUT#.VALUE reads the analog output value.

Examples

Context

For more information see Analog Output.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read Only
Units V
Range 0 to 10V
Default Value 0V
Data Type Float
See Also  
Stored in Non-Volatile Memory No

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AOUT1.VALUE

3800h

01h

Signed16

-

1000:1

Read only

Yes

AOUT2.VALUE

3801h

01h

Signed16

-

1000:1

Read only

Yes

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AOUT1.VALUE

24000

5DC0

Signed16

Read Only

-

AOUT2.VALUE

24001

5DC1

Signed16

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AOUT1.VALUE

24000

Float

Read Only

-

AOUT2.VALUE

24001

Float

Read Only

-